Create points
To create points
- ClickManage Points, and then clickEdit Points.TheEdit Pointspage appears.
- At the bottom of the page, clickNew.
- ThePoint Propertypage appears.
- Fill in the point attributes.For details, see Define point attributes.
- ClickSave.
If the data transfer service is set to the auto transfer mode, the new points will be created with the new tag names automatically. Otherwise, you need to add the new points to the data transfer manually.
To add new points to the data transfer
- ClickConfigure Historian, and then clickData Transfer Points.TheData Transfer Pointspage appears.
- Using the search boxes, find the points that you want to add to the data transfer.
- In the search results table, select the points that you want to add to the data transfer.
- ClickSave.
- In the left pane of the window, clickData Transfer.
- Restart the data transfer service.
Provide Feedback