Configure Trigger Input points
You can associate an Input point with a trigger point by defining the
Extended Description
attribute of the Input point using the following expression:<keyword>='<trigger_tag_name>';<condition>
Where:
This variable | Is |
|---|---|
<keyword> | Either of the following:
|
<trigger_tag_name> | The name of the trigger point. |
<condition> | Any of the following:
|
Any scan tag that is referenced in the
Extended Description
or Scan Tag
point attributes must not be high-speed or have a scan rate higher than 1 second. Otherwise, the module will generate an error and you will not be able to save your point.If you provide an expression in the
Extended Description
point attribute, the point for which you have defined it is considered by the system to be trigger-based rather than scan-based. As a result, an input is triggered when a new value is sent to the snapshot of the trigger point.The TRIG keyword in the expression does not require any condition. Its default condition is
Any
and you cannot change it.The EVENT keyword requires a trigger condition to function properly. If you use multiple trigger definitions, you can separate them with a space, a comma, or a semicolon.
The following table lists the two keywords and their possible values.
Keyword | Trigger condition | This condition triggers an event on | Example |
|---|---|---|---|
TRIG | Any | - | - |
EVENT | Any | - | - |
Nonzero | Any non-zero value. | An event is triggered on a value change from "Pt Created" to 1 but it is not triggered on a value change from 1 to "bad Input". | |
Anychange | Any change as long as the value of the current event is different from the value of the previous event. | An event is triggered on a value change from 0 to "bad Input" or from "bad Input" to 0. | |
Increment | Any increase in the value. | An event is triggered on a value change from 0 to 1. | |
Decrement | Any decrease in the value. | An event is triggered on a value change from 1 to 0. |
Provide Feedback