Differences between upgrade and reinstallation
There are the following differences between upgrading and reinstalling the firmware:
Upgrade
- Updated binary files are installed.
- All log files are deleted.
- The module's configuration data and the archive files are preserved.
Reinstallation
- Updated binary files are installed.
- All log files, module configuration data, and archive files are deleted
- The module's factory settings are restored.
Provide Feedback