Upgrade or reinstall the firmware

You can upgrade or reinstall the firmware of your Historian ME module using
ControlFLASH
or
ControlFLASH Plus®
.
For details on the differences between upgrade and reinstallation, see Differences between upgrade and reinstallation.
The process consists of the following steps:
  1. IMPORTANT:
    If you click
    Restore Defaults
    or
    Reset Security
    from the FactoryTalk Historian ME Logix Designer Module Profile, the module goes into a pending state. The pending state blocks you from upgrading or reinstalling the firmware before one of the following occurs:
    • The five (5) minute window expires.
    • The module is physically reset in the chassis.
    • You power-cycle the module.
    Therefore, you can only upgrade or reinstall the firmware when the module is not in a pending state.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal