Log out of FactoryTalk Historian ME
The reason for this is that after the initial login, when another FactoryTalk-enabled product is started, FactoryTalk Security checks the credentials of the logged-in user at the FactoryTalk Directory, and authorizes access to the next product without requiring another log in.
- ClickLogoutin the upper-right corner of the Historian webpage.
If you close your browser without logging out, a cookie will retain the session for twenty minutes, and another user may access FactoryTalk Historian ME without logging into the module.
It is recommended that every user should log out after every session to help prevent unauthorized users from accessing the module without logging into the module.
Provide Feedback