Access the FactoryTalk Historian ME webpage
FactoryTalk Historian ME
receives data from ControlLogix through the data collection interface and stores it locally in the module. The module data and system information can be viewed and managed through the FactoryTalk Historian ME
webpage. The web interface supports multiple layers of firmware applications that are designed to collect data, as well as provide system and module status and statistics.You can access the
FactoryTalk Historian ME
webpage through a web browser after the installation of the module.Provide Feedback