Restart the module
To restart the module
- Shut down the module.See Shut down the module.
- Click theAdvancedtab, and then clickModule Shutdown.
- Go to the module, and do either of the following:
- Cut off and restore the power to the module by turning off and on the power switch on the chassis.
- Unplug and insert the module into the chassis.
Provide Feedback