Shut down the module
The module shutdown allows you to stop all FactoryTalk Historian ME-related services (including the point server, the data collection, the data transfer, and the web configuration server). It is recommended that you shut down the module if you plan to remove it from the chassis or if you are going to power down the chassis.
To shut down the module
- Click theAdvancedtab, and then clickModule Shutdown.A message appears asking you to confirm the action.
- ClickOK.The module shutdown is complete when the scrolling message on the module displays the module's IP address followed by SHUTDOWN.TIP:Alternatively, you can shut down the module using the FactoryTalk Historian ME Logix Designer Module Profile.For details, see Configure the module properties.
Provide Feedback