Change a ladder diagram instruction
    Change a tag value in a ladder element operand that has parameters. You can change an operand that displays a caret. You cannot change the End rung. Positioning the insertion point on the End rung disables editing. 
Prerequisites
To change a ladder diagram instruction
- In the ladder diagram, select the instruction.
- Double-click a parameter of a ladder logic instruction operand and enter a new value either:- Manually. If you know the exact spelling of the tag owner and tag, enter the tag manually. Use the format Owner.Tag.
- Using Data Item Browser.
 - In the property, select . .
- InData Item Browser, select the tag. The connection to the tag appears in the format Owner.Tag.TIP: When you enter an existing tag value in a parameter, the download fault files of the operand update automatically.
- (optional) To discard a new parameter value, pressEsc.
 
Provide Feedback