Move a ladder diagram instruction
    Move a ladder diagram instruction in a ladder diagram routine to have the instruction execute at a different time in the routine. 
Prerequisites
To move a ladder diagram instruction
- In the ladder diagram, drag the instruction to a valid drop zone:- If the caret appears on the Mnemonic operand, you drag the entire instruction.
- If the caret appears on an instruction operand, you drag the instruction field
- If you select multiple instructions, you drag all of the instructions regardless of the caret location.NOTE: Valid drop zones are indicated by . .
 
Provide Feedback