Add a ladder diagram branch level
    Add a branch level to add an additional level to an existing ladder diagram branch. Instructions that you place in a branch level instruct the routine to use either the instruction in the branch level or the instruction in another branch level. 
Prerequisites
To add a ladder diagram branch level
- In the ladder diagram, select a branch.
- From the Ladder EditorToolbox, dragBranch Level to a valid drop zone in the rung. Valid drop zones are indicated by to a valid drop zone in the rung. Valid drop zones are indicated by .
            TIP: IfToolboxis not open, in the pane bar, select .
            TIP: IfToolboxis not open, in the pane bar, select Toolbox. Toolbox.
Provide Feedback