Ladder Editor
    Use the Ladder Editor to edit ladder diagram routines. The Ladder Editor displays a tab for each open routine. 
The Ladder Editor displays the elements in the ladder diagram logic routines: 
- rungs
- branches
- instructions
- operands
- Select the online icon to display the online view. to display the online view.
- Select the offline icon to display the offline view. to display the offline view.
In the online view, a green rail appears at the top of the routine and the  at the top right lights up.
 at the top right lights up. 
Online
 chip  at the top right lights up.
 at the top right lights up. When logic is executing, a green rail appears on the left and right sides of the rungs in the routine.
The online chip can also indicate a project mismatch or a disconnected state.
     TIP: 
    In the online view, ladder logic is read-only and cannot be edited.
A caret on the Ladder Editor canvas indicates the working position in the routine. The caret only appears when the view is active. When a routine first opens, the caret appears in the rung selection region of the first rung.
     TIP: 
    At the top of the Ladder Editor:
        
- ?indicates where to enter a parameter value for the instruction.
- ??indicates that the system was unable to supply a value for a parameter because the system was unable to attain the value from the Tag Editor.
Provide Feedback