Edit the parameters for the definition of an Add-On Instruction
    Edit parameters for the definition for an Add-On Instruction to change the tag or any of the tag parameters. All changes to a tag are propagated throughout the Add-On Instruction instances. 
- On the explorer bar, select Library. Library.
- InLibrary, right-click the Add-On Instruction and selectTags and parameters. The Tag Editor opens.TIP: To openTags and parameters, you can also select the Add-On Instruction inLibraryand then in theLibrarytitle bar, select View tags and parameters: (item name). View tags and parameters: (item name).
- In the Tag Editor, change any cell in the row of a tag to change:- Name. Type the name of the tag or program parameter.
- Data Type. Type the name of the data type until the data type appears or browse to openSelect Data Type, select the data type from the list, and then selectApply.
- Value. Enter the value of the tag.
- (Optional)Description. Enter a description of the tag to indicate the purpose of the tag or the latest change to the tag.
- Scope. The scope of the tag. The scope is read-only and determined by the item inSystemfrom which you openTags and parameters.
- (Optional)Style. For a BOOL, SINT, INT, DINT, or REAL tag, select a display style to define how the tag value appears. Styles include BINARY, DECIMAL, HEX, OCTAL, ASCII, EXPONENTIAL, FLOAT.
- Usage. Select a usage type -- LOCAL, INPUT, OUTPUT, or INOUT.TIP: Select a tag in the Tag Editor to edit the parameters of the tag inProperties.
 
Provide Feedback