Edit the definition of an Add-On Instruction
    Edit the definition of an Add-On Instruction to change the name, description, vendor, version number or version notes for an Add-On Instruction or to add or delete a scan mode. Edit the Add-On Instruction definition from the Add-On Instruction or an instance of the Add-On Instruction. Changes made to the definition of an Add-On Instruction affect all instances of the Add-On Instruction in the project. 
- On the explorer bar, select Libraryand then double-click the Add-On Instruction. The definition of the Add-On Instruction opens. Libraryand then double-click the Add-On Instruction. The definition of the Add-On Instruction opens.
- UnderGeneral,configure:- Date type size.The size of the date, in bytes, of the Add-On Instruction. Data type size is read-only.
- Name.Type a new name for the Add-On Instruction.
- Description. Type the description of the task that the Add-On Instruction performs.
- Vendor. Type the owner of the Add-On Instruction.
- Type. The Ladder Diagram type is read-only.
 
- UnderScan modes, add or delete a scan mode:- Prescan. Create a routine for the Add-On Instruction that executes before the first scan changes from Program mode to Run mode for the Add-On Instruction. SelectCreate prescan routine, enter an optionalDescriptionand then selectOK.Prescanappears under the Add-On Instruction in theLibrary.TIP:- Select the prescan routine inLibraryto add logic to or edit logic in the routine.
- If a prescan routine exists for the Add-On Instruction, selectDelete prescan routineto delete the prescan routine before creating a routine.
 
- EnableInFalse. Create a routine for the Add-On Instruction that executes when the EnableIn parameter is false. SelectCreate EnableInFalse routine, enter an optionalDescriptionand then selectOK.Prescanappears under the Add-On Instruction inLibrary.TIP:- Select theEnableInFalseroutine inLibraryto add logic to or edit logic in the routine.
- If anEnableInFalseroutine exists for the Add-On Instruction, selectDelete EnableInFalse routineto delete the EnableInFalse routine before creating a routine.
 
 
- UnderVersion, enter:- Version number. Enter theMajor,Minor, andBuildversions for the Add-On Instruction. The maximum number for each version is 999.
- Version note. Enter a description of the version.
 
Provide Feedback