Replace a Redundant Module
To replace a redundant module, refer to one of the following procedures in Module Replacement:
- Perform a direct module replacement in the secondary chassis
- Perform a communication module series replacement
- Perform a redundancy module catalog number replacement
Provide Feedback