Set Up a Redundant Chassis Pair
The setup process of a redundant chassis pair consists of the following:
- Firmware bundle installation
- FactoryTalk® LinxRedundancy Module Configuration Tool (RMCT) installation
- Redundant chassis component installation and firmware updates
- Identification of the primary and secondary chassis
- Qualification and synchronization verification
After setup, you can reset, remove, and replace redundancy modules as needed.
Before You Begin
Before you begin, do the following:
- Make sure that the redundant chassis pair has the required matching components. For best performance, place the redundancy module in the chassis as close as possible to the controller.
- Read and understand the safety and environmental considerations explained in the installation instructions for each component.
- Download and install the compatible versions of theStudio 5000 Logix Designer®application, communication software, andControlFLASH Plus®software. For information on how to download and installControlFLASH Plus®software, see the ControlFLASH Plus Quick Start Guide, publication CFP-QS001.IMPORTANT: If communication software is already on your system, be sure to shut it down before you install or update software.
- Review the release notes for the firmware bundle that you are installing. Make sure that you have compatible hardware and the correct firmware revisions.
- Determine the IP address for each of your Ethernet/IP™ communication modules. Both communication modules in the redundant chassis pair usually have the same IP address. See IP Address Swapping.
Provide Feedback