Store a Project While the System is Running

To store your controller project in nonvolatile memory while your redundant system is running, complete these steps.
  1. Access the RMCT.
  2. Verify that the redundant chassis are synchronized.
  3. On the Configuration tab, set Auto-synchronization to Never.
  4. On the Synchronization tab, select Disqualify Secondary.
  5. Go online with the secondary controller.
    IMPORTANT:
    Do not go online with the primary controller until you have completed this procedure.
  6. In the Logix Designer application, access the Controller Properties dialog box and select the Nonvolatile Memory tab.
  7. To store the project in nonvolatile memory, select Load/Store then <--Store.
  8. Access the RMCT.
  9. On the Synchronization tab, select Synchronize Secondary and wait for the system to synchronize.
  10. Select Initiate Switchover.
  11. Go online with the new secondary controller.
  12. To store the project, complete step 6 and step 7.
  13. On the Configuration tab of the RMCT, set Auto-synchronization to your preferred setting.
  14. On the Synchronization tab, select Synchronize Secondary.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal