Store a Project to the Memory Card

Use this procedure to store an updated project and firmware to the memory card in the controller. You can store a project to the memory card in either of these conditions:
  • Store a project with the controller in Program or Remote Program mode
  • Store a project while a system is running
IMPORTANT:
We recommend that you store the same project on the memory cards in both controllers. Then, if a primary or secondary controller loses the project from its internal memory, you can load the most recent project back onto that controller.
If you store the same project on the memory cards of both controllers while the process is running, you must save the project on the controllers while they are in the secondary controller state. To do so, you save the project on the secondary controller, conduct a switchover, and save the project on the new secondary controller. Even if you do not plan to use the memory card, leave the card installed in the controller to collect diagnostic information that you can provide to Rockwell Automation Technical Support.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal