Monitor and Maintain Redundancy
To monitor and maintain redundancy, you can do the following:
- Reference the controller log
- Track changes to components, such as routines and Add-On Instructions
- Use logic to monitor status
- Monitor communication module statistics
- Understand temperature monitoring and fault behavior
Provide Feedback