Create an embedded database

Create an embedded database

Create an SQLite database embedded in your project. Typically, embedded databases manage data supporting other objects within the
FTOptixApplication
.
  1. In
    Project view
    , right-click
    DataStores
    and select
    Embedded database
    .
  2. (optional) In
    Properties
    , in
    Filename
    , enter a custom name for the database file.
  3. Set
    In memory
    to either:
    • True
      . Makes the database non-persistent. The stored data is removed when you restart the
      FactoryTalk Optix Application
      .
    • False
      . Makes the database persistent. The stored data is kept when you restart the
      FactoryTalk Optix Application
      .
(optional) Configure the database structure. See Configure a database table.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal