Database

Database

Use database objects to define project-embedded databases or an external databases.

Database types

FactoryTalk Optix Studio
supports the following database types.
Supported database types
Object
Description
Embedded database
An object that represents an SQLite database internal to the project at runtime. You typically use an Embedded Database object to manage data supporting other objects within the
FTOptixApplication
.
An embedded database has no read/write limits.
TIP: An embedded database supports up to 2000 table columns.
ODBC database
An object that represents a local or remote database supported by the Open Database Connectivity (ODBC) protocol. You can use ODBC to query or populate a remote database maintained with other systems that contains data for the project.
Depending on the access management policy of an external database, the external database can have read/write limits.
Influx database
An object that represents a remote Influx database, especially useful for time series data. In a limited way, you can use SQL to query or populate a remote database maintained with other systems that contains data for the project.
TIP:
FactoryTalk Optix Studio
parser can transform only some SQL commands to InfluxQL (Influx query language). See Influx database limitations.
Depending on the access management policy of an external database, the external database can have read/write limits.
For more information, see Create a remote Influx database.

Use of databases

You can read from and write to a database through:
Examples of objects that can interact with a database
Object
Database interaction
Data grid
Query a database to obtain data to be displayed at runtime. For example, display database records from a specific date in a Data grid.
List box
Combo box
Trend
Data logger
Write data
Event logger
Recipe schema
Write and read data
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal