Settings
    The owner or administrator of an organization can edit their organizations by selecting 
Settings
 in the FactoryTalk Hub menu.From the Organization Settings screen you can:
- Change the name, description, location and add an image of the organization.TIP: Images used for organization logos must be smaller than 125 kB.
- Transfer organization ownership if you do not want to be an owner of an organization. Only the owner can transfer the ownership. See Transfer Organization Ownership.
- Leave organization that you do not want to be a member of. The owner of the organization cannot leave the organization before transferring the ownership. See Leave an Organization.
- Set an organization to be publicly visible or not by selecting the Organization Access checkbox. Leaving the box unchecked means only people who receive an invitation or Join request link you have shared can see and join your organization. A user can modify a email domain for an organization and add more that one domain.TIP: Any set of email domains configured means that when the organization is publicly visible, all users having any of those email domains can see it in the Join organization page and request access to it.
- Create and copy new Join Links to let people request access to the organization. When you reset a link from an organization's edit organization page, all previous links to the page become invalid.
- You can archive organizations that are no longer in use, or that you created by mistake. See Archive Organization
Provide Feedback