Transfer Organization Ownership
    As an owner of an organization, you can transfer organization ownership to another
      user.
- From the FactoryTalk Hub menu, selectOrganizations.
- From the list of organizations, select the organization which ownership you want to transfer.
- From the FactoryTalk Hub menu, selectSettings.
- In the Owner section, selectTransfer ownership.
- When prompted, verify the applications ownership you want to transfer and provide the name of a new owner.TIP: A new owner must be a member of the organization which ownership you want to transfer.
- SelectTransfer.You are no longer the owner of the organization.
Provide Feedback