Configure output limits

Create a channel-level configuration specific to your application.
Use the
Limits
view to set clamping and ramp limits that prevent damage to equipment.
To configure output limits on an analog output device
  1. On the tab for the device, expand
    Channels
    or
    Output Channels
    , and then expand an individual channel.
  2. Select
    Limits
    .
  3. In the
    Limits
    view, customize the parameters as needed.
  4. Select
    OK
    to save the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal