Limits view

Use the
Limits
view to configure output limits on the 1756-OF4 and 1756-OF8 analog output devices operating in floating point mode and on the 1756-IF4FXOF2F analog device. Set clamping and ramp limitations that prevent damage to equipment.
Use the
Limits
view to:
  • Enter clamp limits.
  • Enable ramping in Run mode.
  • Enter a ramp rate.
  • Disable or latch clamp alarms.
  • Maintain the high and low limit alarms even after the condition ceases.
  • Maintain the rate alarm even after the condition ceases.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal