Alarms view

Use the
Alarms
view to configure process and rate alarms on non-isolated analog input devices. Configure alarms on a per-channel basis.
The
Alarms
view is not available when
Connection
is set to
Listen Only Data
. For 1756-IF8 and 1756-IF16 specifically, to make the
Alarms
view available,
Data Format
must be set to
Float
as well.
Use the
Alarms
view to:
  • Set high and low limits for process alarms
  • Set a trigger value for a rate alarm
  • Disable alarms
  • Latch and unlatch alarms
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal