You may also be interested in
Global offshore energy operator that manages nine water injection platforms, supports reservoir pressure, and optimizes oil and gas production.
- Need for modernization of monitoring and control systems across nine offshore platforms within 24-week timeline
- Complex coordination across multiple vendors and system integrators
- Limited access to remote offshore locations, increasing logistical complexity
- Need to integrate diverse legacy control and power systems
- Challenges implementing reliable satellite-based monitoring across all sites
- ControlLogix® and FLEX I/O® architectures
- CENTERLINE® 2100 Motor Control Centers across all platforms
- PowerFlex® 755T-series Variable Frequency Drives
- Satellite-based monitoring
- FactoryTalk® View
- Studio 5000®
- FactoryTalk® Historian
- Operationalized five offshore platforms within project timeline
- Reduced manual intervention through centralized monitoring and control capabilities
- Improved operational efficiency and system reliability in harsh offshore conditions
- Enhanced real-time data visibility across all connected platforms
- Achieved high client satisfaction with scalable, future-ready system architecture
Complex Modernization Project Under Tight Deadline
An offshore energy operator needed to modernize monitoring and control systems across nine water injection platforms within a 24-week delivery window. These systems were critical to maintaining consistent reservoir pressure and protecting reliable offshore production operations. The accelerated timeline required rapid execution while maintaining operational continuity.
The remote offshore locations increased the complexity of the project significantly. Limited accessibility and harsh environmental conditions made system installation, commissioning, and maintenance more difficult. Transporting equipment and coordinating personnel across multiple platforms required careful planning and execution.
Multi-Vendor, Multi-System Coordination
The project required coordination between multiple suppliers and system integrators, particularly for Motor Control Centers (MCCs) and Variable Frequency Drives (VFDs). Supporting compatibility between different technologies and maintaining alignment across teams introduced additional risk to the project schedule.
Additionally, existing infrastructure included a mix of legacy control and power systems that needed to be unified into a single, cohesive architecture. The operator required a solution that would integrate these systems while improving overall performance and scalability.
Need for Remote Visibility
Finally, frequent on-site visits were inefficient and costly. The operator needed reliable remote monitoring capabilities to gain real-time visibility into operations, reduce manual intervention, and improve decision-making across all offshore facilities.
A Cohesive Solution Optimized for Success
The energy operator implemented a unified automation solution designed to integrate control systems across all nine offshore platforms. The architecture leveraged ControlLogix® and FLEX I/O® technologies to provide a scalable and flexible foundation.
Each platform was equipped with CENTERLINE® 2100 Motor Control Centers, delivering consistent and reliable power management across the operation. These systems were seamlessly integrated into the broader control environment to best coordinate performance.
To optimize performance and improve operational precision, the operator chose PowerFlex® 755T-series VFDs. These drives provided precise control of motor speed and torque, improving efficiency and supporting stable water injection processes.
Integrated offshore control system supporting remote monitoring and control across multiple water injection platforms
Real-Time Monitoring and Standardization
A key component of the solution was the implementation of a satellite-based monitoring system. This capability delivered real-time communication between offshore platforms and centralized operations, providing operators with full visibility into system performance.
Finally, the control solution incorporated a comprehensive software suite, including FactoryTalk® View, Studio 5000®, and FactoryTalk® Historian. These tools provided advanced visualization, control, and data management capabilities, allowing workers to capture and analyze performance data across all platforms.
Improved Operational Efficiency, Visibility, and Reliability
The implementation of the integrated control and monitoring system improved operational efficiency across all offshore platforms. With centralized oversight, the solution reduced the need for manual intervention and allowed workers to manage systems more effectively from remote locations.
The satellite-based monitoring system provided real-time access to operational data, giving workers greater visibility into system performance. This enhanced insight supported faster decision-making and improved responsiveness to changing conditions.
The robust system architecture improved reliability across offshore operations, even in challenging environmental conditions. Standardized control systems and advanced motor control technologies helped deliver consistent and dependable performance.
Scalable, Future-Ready Infrastructure
The solution created a scalable foundation that supports future expansion and integration. The unified architecture allows the operator to extend capabilities across additional platforms and adapt to evolving operational requirements.
Five of the nine platforms were successfully operationalized within the project scope. The operator reported high satisfaction with the system’s performance, highlighting its ability to transform complex technical challenges into sustainable, long-term operational advantages.
Published June 30, 2026