Syslog Routing Settings
    Below are settings for enabling and configuring Syslog in 
FactoryTalk® Policy Manager
.Syslog routing
      
  Property  | Description  | 
|---|---|
Enable syslog routing using syslog server  | Enables devices that support syslog routing to start sending Syslog messages as configured in the policy. These settings apply to all devices that support syslog routing.  | 
 Property  |  Description  | 
|---|---|
IP Address  | Identifies the Syslog server by the IP address.  | 
Hostname  | Identifies the Syslog server by the DNS host name.  | 
Port  | Identifies the communications port on the server to receive the Syslog messages. Default port number is 514.  | 
Protocol  | Configures logging.
                   
  | 
 Property  |  Description  | 
|---|---|
Event types that will generate messages  | Used to determine which event types generate messages.
                   
  | 
Lowest level of severity to log  | Logs messages that are greater than or equal to the severity level selected. Defined severity levels from highest to lowest are:
                   
  | 
 Property  |  Description  | 
|---|---|
Details to include in message  | Specifies details included in the message.
                   
  | 
Time resolutions  | Defines the level of precision used in the time stamp of the log messages:
                   
  | 
Provide Feedback