Syslog Technology
    Syslog is a standardized and widely used event message logging technology. Syslog is used to generate, store, report, and analyze security-related events.
When Syslog operates over a network, it uses a client-server architecture in which a syslog server monitors for, and logs, messages that are coming from clients.
The following products support Syslog:
        
- FactoryTalk® Linxsoftware, version 6.21 or later
 - ControlLogix®5580 controllers, firmware revision 34.011 or later
 - ControlLogix®5590 controllers, firmware revision 38.011 or later
 - GuardLogix®5580 controllers, firmware revision 34.011 or later
 - 1756-EN4TREtherNet/IP™communication module, firmware revision 4.001 or later
 - 1783-CSPCIP Security™Proxy, firmware revision 1.001 or later
 - PowerFlex®755T drives, firmware revision 10.001 or later
 - PowerFlex®6000T drives, firmware revision 10.001 or later
 
     IMPORTANT: 
    
CIP Security™
-capable devices are Syslog-capable. To enable and configure Syslog in certified security applications, you must implement CIP Security™
.However, Syslog is not exclusive to industrial automation control systems that use 
CIP Security™
. You can also use Syslog in applications that aren't certified security applications, and with 
CIP Security™
-capable devices when CIP Security™
 is not enabled on the devices.For more information on Syslog, see the following:
        
- Syslog Status Messages Reference Data, publication SYSLOG-RD001
 
Syslog Collector
      A Syslog collector stores event messages that are sent from the generating device to the collector.
When you choose a Syslog collector tool, it must support the following:
        
- RFC-5424 Syslog protocol
 - Ability to receive messages fromCIP Security™-enabled devices
 
Provide Feedback