Edit an AOI with existing
FactoryTalk Smart Object
instances

Upon its creation, an Add-On Instruction inherits values from the definition. After Add-On Instruction creation, manually push new Add-On Instruction definition changes to the instances of the Add-On Instruction with
FactoryTalk Smart Object
instances.
To edit an Add-On Instruction with existing
FactoryTalk Smart Object
instances
  1. Select
    Configure AOIs
    .
  2. Select an Add-On Instruction.
  3. Perform one of these actions:
    • Right-click the information model and then add a data type or node.
    • Right-click the Add-On Instruction. Select
      Properties.
      Change the name and then select
      Update
      .
  4. Verify that the Add-On Instruction model is correct.
  5. In
    Studio 5000 Logix Designer
    , go to the logic of the Add-On Instruction and then monitor a tag.
  6. In
    Copy default values to tags of type
    , select
    Copy Specified Values
    .
  7. Select the local tag for the modified
    FactoryTalk Smart Object
    and then select
    OK
    .
  8. Download the
    Studio 5000 Logix Designer
    project to a controller or emulator.
  9. Put the controller in Run mode for at least 5 seconds. Save and then upload the values.
  10. In
    Studio 5000 Smart Object Configurator
    , select
    Refresh information model
    .
    The information models reflect the changes.
    TIP:
    To delete a
    FactoryTalk Smart Object
    inside an Add-On Instruction, in
    Studio 5000 Logix Designer
    delete the code and backing tag. Reconnect
    Studio 5000 Smart Object Configurator
    . There is no need to download the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal