Create a node
Use nodes to organize
FactoryTalk Smart Object
instances and to define how FactoryTalk Smart Object
instances are collected. A node does not sample a specific tag’s value but instead defines the data collection mechanism for its children. A node exists only as a folder in a hierarchy to provide structure for the information model. To create a node, set the node properties and then set the data collections parameters. Node properties are saved in the .acd project file and define basic information regarding the node.
Data collection parameters define how data is collected for
FactoryTalk Smart Object
instances that are under a node that collects data based on the Parent parameter. When data collection definition includes the Parent parameter, data collected for a hierarchy based on this setting collects in the same controller scan and has synchronized time stamps. Data collection in
Studio 5000 Smart Object Configurator
is hierarchical and by default data collection is based on the top level in the model. Break and re-establish the link between each node and its parent by using the Parent parameter in the data collection configuration.To create a node
- Perform one of these actions:
- To add the first node, right-click an information model and then selectNew Node.
- To add a node under another node, right-click a node and then selectNode.
- To add a node under another node, selectAdd
and then select
Node.
- Set these basic properties:
- Name: Name of the node displayed in the information model. See Rules for names and backing tags.
- Backing tag: Name of the backing tag created in the controller. A backing tag is created in theStudio 5000 Logix Designerproject that contains the configuration information for theFactoryTalk Smart Object.
- Program: Controller program where the node resides.
- Routine: Controller routine where the node resides.
- Insert at: Location to add a rung in the routine where theFactoryTalk Smart Objectappears.
- Insert at end: Location at the end of the routine where theFactoryTalk Smart Objectappears.
- Set these data collection parameters:
- On parent or periodic: When this checkbox andOn programmaticcheckbox is clear, data collection for this node does not occur.TIP:The first node should have On programmatic trigger or Periodic data collection parameters because it does not have a parent.It is possible to have multiple triggers active at once. Possible trigger combinations are: Parent trigger and On programmatic trigger or Periodic and On programmatic trigger.
- Parent: When the parent is triggered, theFactoryTalk Smart Objectis also triggered.
- Periodic: Interval seconds at which point data is sampled in the source tag.
- On programmatic: Ladder logic that triggers the condition for collection.
- (Optional) UnderInformation attributes, selectThingWorx template, and then type the name of the template to use for this node when mapping this model to a ThingWorx instance.TIP:The ThingWorx template:
- Cannot exceed 256 characters.
- Cannot contain three colons in a row (:::) or an ellipsis (...).
- Cannot begin or end with a period (.) or a colon (:).
- SelectAdd. The node appears in theFactoryTalk Smart Objectinformation model.
Provide Feedback