About the
SequenceManager
Controls

The
SequenceManager
Controls are divided into functional areas:
  • Sequence Detail Control
    The
    Sequence Detail Control
    provides the operator with a detailed view of an Equipment Sequence, including its chart structure, steps, and transitions. The runtime status of the sequence program and its sequence elements are also shown. The operator can command the Equipment Sequence from this control.
  • Sequence Summary Control
    The
    Sequence Summary Control
    displays the sequence program status for each of the Equipment Sequences downloaded to the controller. The Sequence Summary Control also allow the operator to view and command a selected Equipment Sequence.
  • Sequence Parameters Control
    The Sequence Parameters Control displays a table of all sequencing parameters and step tags of a specified ES, and allows the operator to command a selected sequencing parameter or step tag. To refine the display, configure the table to filter the information displayed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal