Introduction
The
SequenceManager
Visualization Components includes the FactoryTalk® View Site Edition (SE)
ActiveX Controls and the SequenceManager
Server Service.The
SequenceManager
ActiveX Controls sequences a series of Equipment Phase
s to the Control Logix platform. The operator views and interacts with the Equipment Sequence
s downloaded to a Logix controller through three types of controls: - Sequence Detail Control
- Sequence Summary Control
- Sequence Parameters Control
The
SequenceManager
Server Service application is a SequenceManager
component for operator visualization and interaction. The SequenceManager
Server Service application makes controller data available to the ActiveX Controls and allows the operator to command sequences. If the SequenceManager
Server Service application is not running, SequenceManager
ActiveX Controls will not display data.SequenceManager
controls can only be embedded with FactoryTalk View SE
displays.Provide Feedback