HeartbeatRate property

Returns or sets the maximum rate, in milliseconds, between updates when a chart is updating on change. Read/write. Long.
Use this property with the ChartMode property set to rstOnChange.
Syntax
Trend
.
HeartBeatRate
[
= vlalue
]
where
Trend
- is the name of a Trend object (such as trend1) or an expression that evaluates to a Trend object.
value
- is a parameter of the type Long that specifies the maximum rate. Limits are 0 or 1000 - 1800000000.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal