ChartMode property

Returns or sets how often the chart updates data, using one of three modes:
Manual
,
Automatic
, and
On Change
. Read/write. Constant.
Syntax
Trend
.
ChartMode
[
= chartMode
]
where
Trend
- is the name of a Trend object (such as trend1) or an expression that evaluates to a Trend object.
chartMode
- is a constant of the type RSTchartModes. It can be Manual, Automatic, or On Change.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal