DataServer property
Returns or sets a server that provides data outside of the automation interface. Read/write. Constant.
Syntax
Trend
.DataServer
[ = rstdataServer
]where
Trend
- is the name of a Trend object (such as trend1) or an expression that evaluates to a Trend object.rstdataServer
- is a constant of the type RSTdataServer.Provide Feedback