RSTdataServer constants

The following constants are defined:
Constant
Description
rstDataServerNone
The automation interface provides and updates chart data, as specified by the ChartMode property. This setting applies to most containers.
rstDataServerAcquirer
The trend object will acquire data from the container. This setting does not apply to most containers since most containers provide the chart with data.
rstHistoricalPoll
The trend object will poll for the newest historical data. This setting applies only to FactoryTalk View Site Edition.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal