SignatureButtonOperations constants
The following constants can be returned or set by the Operation property.
- SetValue(1) – specifies that the operation the SignatureButton is to perform is to set the Value property of the numeric tag associated with the button in the Connections tab.
- RunCommand(2) – specifies that the operation the SignatureButton is to perform is to run a command.
- DownloadInputValues(3) – specifies that the operation the SignatureButton is to perform is to download values from all the input fields on the current display.
- SetString(4) – specifies that the operation the SignatureButton is to perform is to set the Value property of the string tag associated with the button in the Connections tab.
- SetDateTime(5) – specifies that the operation the SignatureButton is to perform is to set the DatePart, TimePart, or DateTimeString property of the tag associated with the button in the Connections tab.
- SetBoolean(6) – specifies that the operation the SignatureButton is to perform is to set the Value property of the boolean tag associated with the button in the Connections tab.
Provide Feedback