Operation property
Returns or sets the operation the signature button will perform at runtime when it is pressed. Read/write.* Constant.
Syntax
object
.Operation
[ = type]where
object
– is the name of a SignatureButton object or an expression that evaluates to a SignatureButton object.type
– is a constant of the type SignatureButtonOperations that specifies the operation the button will perform when it is pushed.Remarks
- *When the electronic signature window is open at runtime, in other words when a signature authentication operation is taking place, this property is read-only.At runtime when the electronic signature window is not open (no signature authentication is taking place) the property is read/write.This means that you can use VBA code to make changes to the signature button properties at runtime, as long as the electronic signature window is not open.
Provide Feedback