VerticalScaleFactor property

Returns a value that is used to calculate the pixel value of a vertical measurement when a display has been scaled (resized). The value of this property is 1 if the display is not scaled. Read-only. Single.
Syntax
Display
.
VerticalScaleFactor
where
Display
– is the name of a Display object or an expression that evaluates to a Display object.
Remarks
Multiply DisplayAreaHeight by VerticalScaleFactor to get the actual height of the display region in pixels.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal