Height property (Display object)

Returns or sets the external height of the display window, in pixels, including the borders and title bar. Read/write. Long.
If a display is docked, this property is read-only.
The value assigned to this property must be greater than or equal to 27.
Syntax
Display
.
Height
[ =
value
]
where
Display
– is the name of a Display object or an expression that evaluates to a Display object.
value
– is the external height, in pixels, of the display.
Remarks
  • The value of this property can be changed even if the option
    Size to Main Window at Runtime
    is specified or the option
    Allow Display to be Resized
    is not specified.
  • When the display is minimized, the height changes to match the height of the window icon in the lower left portion of the containing window.
  • When the display is maximized, the height changes to match the height of the containing window.
  • If you attempt to move or size a display that is minimized, maximized, or docked, the error gfxErrorMoveResize is raised.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal