RootFolder property

Returns a Folder object that represents the root folder of the HMI tag database. Read-only.
Syntax
TagDB
.
RootFolder
where
TagDB
is the global variable
TagDB
. You can also use a variable you have defined as a TagDB object or an expression that evaluates to a TagDB object.
TIP:
If you are not using
FactoryTalk View SE
's VBA, the global variables will not be automatically created and you will have to define your own object variables.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal