Example: Get all folders under the root folder

This example prints the names of all folders in the root folder in the tag database.
Sub ShowSubFolders() Dim oFolders As Folders Dim oFolder As Folder 'Get the folders in the Root folder. Set oFolders = TagDB.RootFolder.Folders Debug.Print Debug.Print "The Root folder contains the following sub-folders:" Debug.Print 'Print the name of each folder in the collection. For Each oFolder In oFolders Debug.Print vbTab & oFolder.Name Next oFolder 'Release resources associated with the objects. Set oFolders = Nothing Set oFolder = Nothing End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal