Remove method
Removes the tag object specified by Index.
The value of Index can be between 1 and Count, inclusive, or the name of a tag.
Syntax
Group
.Remove
(Index
)where
Group
– is the name of a TagGroup object or an expression that evaluates to a TagGroup object.Index
– is a parameter of the type Variant that specifies the tag to be removed. The value of Index can be between 1 and Count, inclusive, or the name of a tag. Relative names are resolved using the HomeAreaName property value.Remarks
If the tag is not found in the group, the error tagErrorCollectionIndex is raised.
Provide Feedback