HomeAreaName property
Returns the name of the area. The name is used to resolve a relative tag reference into a fully qualified tag reference when the tag is added to a collection. Read-only. String.
Syntax
Object
.HomeAreaName
where
Object
is the name of a FactoryTalk View SE
object or an expression that evaluates to a FactoryTalk View SE
object.Remarks
This property is set when a TagGroup is created, and is the home area of the display in which the TagGroup is created.
Provide Feedback