Fully qualified name

Fully qualified name is a name that specifies the complete path to the named object from the root of the application.
The following example is the fully qualified name of the display named
Line Overview
.
/Mixing Plant/Mixing Line1::Line Overview
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal