QoS property
Gets or sets the subscription QoS level. Read/write.
Syntax
subOption
.QoS
where
subOption
- is an MQTTSubscribeOption object created by the MQTTFactory object's method CreateSubscribeOption
.Default value
If this property is omitted, it will use its default value, which is
MqttQoSLevel_AtMostOnce (0)
, meaning the message arrives at the receiver either once or not at all.Provide Feedback