MQTTSubscribeOption object
The MQTTSubscribeOption object contains the parameters required for a subscription. MQTT allows clients to use different subscription options for each of their subscriptions.
When an MQTT client needs to subscribe to a topic, it can create an instance of the subscription option through an MQTTFactory method.
Properties
Provide Feedback