Symbol object
The Symbol object represents the intrinsic Symbol object. It is not a creatable object. Symbol objects are accessible through an Elements collection.
The Symbol object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback