Scale object

The Scale object represents the intrinsic Scale object. It is not a creatable object. Scale objects are accessible through an Elements collection.
The Scale object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal